Proficy Historian Client Access API
Proficy.Historian.ClientAccess.API Namespace / Collector Class / ShouldQueueWrites Property



In This Topic
    ShouldQueueWrites Property
    In This Topic
    Whether data samples are queued and written as a single batch-write to a Historian server. Queuing data writes more efficiently utilizes network resources at a cost of latency in how promptly current data values are recorded in a server.
    Syntax
    'Declaration
     
    Public Property ShouldQueueWrites As Boolean
    'Usage
     
    Dim instance As Collector
    Dim value As Boolean
     
    instance.ShouldQueueWrites = value
     
    value = instance.ShouldQueueWrites
    public bool ShouldQueueWrites {get; set;}
    public:
    property bool ShouldQueueWrites {
       bool get();
       void set (    bool value);
    }
    Requirements

    Target Platforms: Windows 7, Windows Vista SP1 or later, Windows XP SP3, Windows Server 2008 (Server Core not supported), Windows Server 2008 R2 (Server Core supported with SP1 or later), Windows Server 2003 SP2

    See Also