Proficy Historian Client Access API
Proficy.Historian.ClientAccess.API Namespace / EnumeratedSet Class
Members



In This Topic
    EnumeratedSet Class
    In This Topic
    Represents details of an Enumerated Set.
    Syntax
    'Declaration
     
    <DataContractAttribute("EnumeratedSet")>
    <KnownTypeAttribute(Proficy.Historian.ClientAccess.API.Tag/NativeDataType)>
    <SerializableAttribute()>
    Public Class EnumeratedSet 
    'Usage
     
    Dim instance As EnumeratedSet
    [DataContract("EnumeratedSet")]
    [KnownType(Proficy.Historian.ClientAccess.API.Tag/NativeDataType)]
    [Serializable()]
    public class EnumeratedSet 
    [DataContract("EnumeratedSet")]
    [KnownType(Proficy.Historian.ClientAccess.API.Tag/NativeDataType)]
    [Serializable()]
    public ref class EnumeratedSet 
    Inheritance Hierarchy

    System.Object
       Proficy.Historian.ClientAccess.API.EnumeratedSet

    Requirements

    Target Platforms: Windows 7, Windows Vista SP1 or later, Windows XP SP3, Windows Server 2008 (Server Core not supported), Windows Server 2008 R2 (Server Core supported with SP1 or later), Windows Server 2003 SP2

    See Also