Proficy Historian Client Access API
Proficy.Historian.ClientAccess.API Namespace / MultiField Class
Members



In This Topic
    MultiField Class
    In This Topic
    This is the definition of the object contained in the UserDefinedType class.
    Syntax
    'Declaration
     
    <DataContractAttribute("MultiField")>
    <KnownTypeAttribute(Proficy.Historian.ClientAccess.API.Tag/NativeDataType)>
    <SerializableAttribute()>
    Public Class MultiField 
    'Usage
     
    Dim instance As MultiField
    [DataContract("MultiField")]
    [KnownType(Proficy.Historian.ClientAccess.API.Tag/NativeDataType)]
    [Serializable()]
    public class MultiField 
    [DataContract("MultiField")]
    [KnownType(Proficy.Historian.ClientAccess.API.Tag/NativeDataType)]
    [Serializable()]
    public ref class MultiField 
    Inheritance Hierarchy

    System.Object
       Proficy.Historian.ClientAccess.API.MultiField

    Requirements

    Target Platforms: Windows 7, Windows Vista SP1 or later, Windows XP SP3, Windows Server 2008 (Server Core not supported), Windows Server 2008 R2 (Server Core supported with SP1 or later), Windows Server 2003 SP2

    See Also