Proficy Historian Client Access API
Proficy.Historian.ClientAccess.API Namespace / AlarmNotificationInfo Class
Members



In This Topic
    AlarmNotificationInfo Class
    In This Topic
    Represents details of the AlarmNotification Object.
    Syntax
    'Declaration
     
    <DataContractAttribute("AlarmNotificationInfo")>
    <KnownTypeAttribute(Proficy.Historian.ClientAccess.API.AlarmInfo)>
    <SerializableAttribute()>
    Public Class AlarmNotificationInfo 
    'Usage
     
    Dim instance As AlarmNotificationInfo
    [DataContract("AlarmNotificationInfo")]
    [KnownType(Proficy.Historian.ClientAccess.API.AlarmInfo)]
    [Serializable()]
    public class AlarmNotificationInfo 
    [DataContract("AlarmNotificationInfo")]
    [KnownType(Proficy.Historian.ClientAccess.API.AlarmInfo)]
    [Serializable()]
    public ref class AlarmNotificationInfo 
    Inheritance Hierarchy

    System.Object
       Proficy.Historian.ClientAccess.API.AlarmNotificationInfo

    Requirements

    Target Platforms: Windows 7, Windows Vista SP1 or later, Windows XP SP3, Windows Server 2008 (Server Core not supported), Windows Server 2008 R2 (Server Core supported with SP1 or later), Windows Server 2003 SP2

    See Also