Proficy Historian Client Access API
Proficy.Historian.ClientAccess.API Namespace / Collector Class / RedundancyFailoverOnCollectorStatus Property



In This Topic
    RedundancyFailoverOnCollectorStatus Property
    In This Topic
    Whether automatic failover occurs based on collector status in a collector redundancy configuration. When true, a Historian server will initiate failover to a backup collector if the status of the currently active collector changes from StatusType.Running.
    Syntax
    'Declaration
     
    Public Property RedundancyFailoverOnCollectorStatus As Boolean
    'Usage
     
    Dim instance As Collector
    Dim value As Boolean
     
    instance.RedundancyFailoverOnCollectorStatus = value
     
    value = instance.RedundancyFailoverOnCollectorStatus
    public bool RedundancyFailoverOnCollectorStatus {get; set;}
    public:
    property bool RedundancyFailoverOnCollectorStatus {
       bool get();
       void set (    bool value);
    }
    Requirements

    Target Platforms: Windows 7, Windows Vista SP1 or later, Windows XP SP3, Windows Server 2008 (Server Core not supported), Windows Server 2008 R2 (Server Core supported with SP1 or later), Windows Server 2003 SP2

    See Also