Proficy Historian Client Access API
Proficy.Historian.ClientAccess.API Namespace / AlarmBackupResponseHandler Delegate
Whether this is the final response.
Overall operation status.



In This Topic
    AlarmBackupResponseHandler Delegate
    In This Topic
    A delegate invoked for Alarm/Events Backup Response.
    Syntax
    'Declaration
     
    Public Delegate Sub AlarmBackupResponseHandler( _
       ByVal final As Boolean, _
       ByVal status As Status _
    ) 
    'Usage
     
    Dim instance As New AlarmBackupResponseHandler(AddressOf HandlerMethod)
    public delegate void AlarmBackupResponseHandler( 
       bool final,
       Status status
    )
    public delegate void AlarmBackupResponseHandler( 
       bool final,
       Status status
    )

    Parameters

    final
    Whether this is the final response.
    status
    Overall operation status.
    Requirements

    Target Platforms: Windows 7, Windows Vista SP1 or later, Windows XP SP3, Windows Server 2008 (Server Core not supported), Windows Server 2008 R2 (Server Core supported with SP1 or later), Windows Server 2003 SP2

    See Also