'Declaration Public Enum Status Inherits System.Enum
'Usage Dim instance As Status
public enum Status : System.Enum
public enum class Status : public System.Enum
'Declaration Public Enum Status Inherits System.Enum
'Usage Dim instance As Status
public enum Status : System.Enum
public enum class Status : public System.Enum
Member | Description |
---|---|
AccessDenied | Insufficient permissions for operation. |
AlarmArchiverUnavailable | Alarm and Event subsystem unreachable. |
ArgumentException | A supplied argument is invalid. |
ArgumentNullException | A supplied argument is NULL. |
ArgumentOutOfRangeException | A supplied argument is outside the valid range. |
BackupInsufficientSpace | Insufficient disk space to perform backup. |
CircularReference | Circular reference detected in calculation. |
CollectorNotFound | The given collector does not exist on the server. |
DeleteOutsideActiveRange | Attempted data delete outside allowed modification interval. |
DuplicateCollector | The given collector name already exists on the server. |
DuplicateData | Attempt to overwrite an existing data sample. |
Failed | Operation failed. |
InternalLicenseError | Internal license error. |
InvalidCustomDataType | The Custom data type is not supported. |
InvalidDataStore | The requested data store was not found. |
InvalidEnumeratedSet | The requested Enumerated Set was not found. |
InvalidServerVersion | Operation unsupported due to server version. |
InvalidTagname | The requested tag was not found. |
InvalidUsername | Bad user name or password. |
LicensedConnectionCountExceeded | Number of licensed server connections exceeded. |
LicensedTagCountExceeded | Number of licensed tags exceeded. |
NotConnected | Not connected to Historian server. |
NotLicensed | Server or feature is not licensed. |
NotPermitted | Operation not permitted. |
NotSupported | Operation not supported. |
NoValue | No available tag data. |
QueryResultSizeExceeded | Upper limit on query results exceeded. |
Success | Operation successful. |
Timeout | Operation failed due to timeout. |
WriteArchiveOffline | Attempted data write to an offline archive. |
WriteArchiveReadonly | Attempted data write to a read-only archive. |
WriteInFuture | Attempted data write too far in the future. |
WriteNoArchiveAvailable | Attempted data write with no available archives. |
WriteOutsideActiveRange | Attempted data write beyond the configured active range. |
System.Object
System.ValueType
System.Enum
Proficy.Historian.ClientAccess.API.Status
Target Platforms: Windows 7, Windows Vista SP1 or later, Windows XP SP3, Windows Server 2008 (Server Core not supported), Windows Server 2008 R2 (Server Core supported with SP1 or later), Windows Server 2003 SP2