Proficy Historian Client Access API
Proficy.Historian.ClientAccess.API Namespace / MultiFieldValue Class
Members



In This Topic
    MultiFieldValue Class
    In This Topic
    This is the structure of the data written to a tag of type MultiField
    Syntax
    'Declaration
     
    <DataContractAttribute("MultiFieldValue")>
    <KnownTypeAttribute(Proficy.Historian.ClientAccess.API.DetailedValue)>
    <SerializableAttribute()>
    Public Class MultiFieldValue 
    'Usage
     
    Dim instance As MultiFieldValue
    [DataContract("MultiFieldValue")]
    [KnownType(Proficy.Historian.ClientAccess.API.DetailedValue)]
    [Serializable()]
    public class MultiFieldValue 
    [DataContract("MultiFieldValue")]
    [KnownType(Proficy.Historian.ClientAccess.API.DetailedValue)]
    [Serializable()]
    public ref class MultiFieldValue 
    Inheritance Hierarchy

    System.Object
       Proficy.Historian.ClientAccess.API.MultiFieldValue

    Requirements

    Target Platforms: Windows 7, Windows Vista SP1 or later, Windows XP SP3, Windows Server 2008 (Server Core not supported), Windows Server 2008 R2 (Server Core supported with SP1 or later), Windows Server 2003 SP2

    See Also