'Declaration Public Enum CertificateValidationMode Inherits System.Enum
'Usage Dim instance As CertificateValidationMode
public enum CertificateValidationMode : System.Enum
public enum class CertificateValidationMode : public System.Enum
'Declaration Public Enum CertificateValidationMode Inherits System.Enum
'Usage Dim instance As CertificateValidationMode
public enum CertificateValidationMode : System.Enum
public enum class CertificateValidationMode : public System.Enum
Member | Description |
---|---|
ChainTrust | Certificate is considered valid if the certificate chain builds to a certificate authority in the trusted root store. |
None | No certificate validation. |
PeerOrChainTrust | Certificate is considered valid if it appears in the trusted people store, or if the certificate chain builds to a certificate authority in the trusted root store. |
PeerTrust | Certificate is considered valid if it appears in the trusted people store. |
System.Object
System.ValueType
System.Enum
Proficy.Historian.ClientAccess.API.CertificateValidationMode
Target Platforms: Windows 7, Windows Vista SP1 or later, Windows XP SP3, Windows Server 2008 (Server Core not supported), Windows Server 2008 R2 (Server Core supported with SP1 or later), Windows Server 2003 SP2