Proficy Historian Client Access API
Proficy.Historian.ClientAccess.API Namespace / CalculatedQuality Class
Members



In This Topic
    CalculatedQuality Class
    In This Topic
    Represents a computed quality value derived from raw qualities recorded in a Historian server. Calculated quality is a percent value with 100% equivalent to good quality and 0% equivalent to bad quality.
    Syntax
    'Declaration
     
    <DataContractAttribute("CalcQuality")>
    <SerializableAttribute()>
    Public Class CalculatedQuality 
       Implements IDataQuality 
    'Usage
     
    Dim instance As CalculatedQuality
    [DataContract("CalcQuality")]
    [Serializable()]
    public class CalculatedQuality : IDataQuality  
    [DataContract("CalcQuality")]
    [Serializable()]
    public ref class CalculatedQuality : public IDataQuality  
    Inheritance Hierarchy

    System.Object
       Proficy.Historian.ClientAccess.API.CalculatedQuality

    Requirements

    Target Platforms: Windows 7, Windows Vista SP1 or later, Windows XP SP3, Windows Server 2008 (Server Core not supported), Windows Server 2008 R2 (Server Core supported with SP1 or later), Windows Server 2003 SP2

    See Also