Proficy Historian Client Access API
Proficy.Historian.ClientAccess.API Namespace / DetailedValue Class
Members



In This Topic
    DetailedValue Class
    In This Topic
    This class is the individual value contained in the FieldValue.Value
    Object Model
    DetailedValue ClassDataQuality Class
    Syntax
    'Declaration
     
    <DataContractAttribute("DetailedValue")>
    <KnownTypeAttribute(System.Object)>
    <SerializableAttribute()>
    Public Class DetailedValue 
    'Usage
     
    Dim instance As DetailedValue
    [DataContract("DetailedValue")]
    [KnownType(System.Object)]
    [Serializable()]
    public class DetailedValue 
    [DataContract("DetailedValue")]
    [KnownType(System.Object)]
    [Serializable()]
    public ref class DetailedValue 
    Inheritance Hierarchy

    System.Object
       Proficy.Historian.ClientAccess.API.DetailedValue

    Requirements

    Target Platforms: Windows 7, Windows Vista SP1 or later, Windows XP SP3, Windows Server 2008 (Server Core not supported), Windows Server 2008 R2 (Server Core supported with SP1 or later), Windows Server 2003 SP2

    See Also