Proficy Historian Client Access API
Proficy.Historian.ClientAccess.API Namespace / AlarmFields Class
Members



In This Topic
    AlarmFields Class
    In This Topic
    Object Model
    AlarmFields ClassAlarmField ClassAlarmField ClassAlarmField ClassAlarmField ClassAlarmField ClassAlarmField ClassAlarmField ClassAlarmField ClassAlarmField ClassAlarmField ClassAlarmField ClassAlarmField ClassAlarmField ClassAlarmField ClassAlarmField ClassAlarmField ClassAlarmField ClassAlarmField Class
    Syntax
    'Declaration
     
    <DataContractAttribute("AlarmFields")>
    <KnownTypeAttribute(Proficy.Historian.ClientAccess.API.AlarmField)>
    <SerializableAttribute()>
    Public Class AlarmFields 
    'Usage
     
    Dim instance As AlarmFields
    [DataContract("AlarmFields")]
    [KnownType(Proficy.Historian.ClientAccess.API.AlarmField)]
    [Serializable()]
    public class AlarmFields 
    [DataContract("AlarmFields")]
    [KnownType(Proficy.Historian.ClientAccess.API.AlarmField)]
    [Serializable()]
    public ref class AlarmFields 
    Inheritance Hierarchy

    System.Object
       Proficy.Historian.ClientAccess.API.AlarmFields

    Requirements

    Target Platforms: Windows 7, Windows Vista SP1 or later, Windows XP SP3, Windows Server 2008 (Server Core not supported), Windows Server 2008 R2 (Server Core supported with SP1 or later), Windows Server 2003 SP2

    See Also