Proficy Historian Client Access API
Proficy.Historian.ClientAccess.API Namespace / ArrayValue Class
Members



In This Topic
    ArrayValue Class
    In This Topic
    This is the value type for array tags in Historian
    Syntax
    'Declaration
     
    <DataContractAttribute("ArrayValue")>
    <KnownTypeAttribute(Proficy.Historian.ClientAccess.API.ElementValue)>
    <SerializableAttribute()>
    Public Class ArrayValue 
    'Usage
     
    Dim instance As ArrayValue
    [DataContract("ArrayValue")]
    [KnownType(Proficy.Historian.ClientAccess.API.ElementValue)]
    [Serializable()]
    public class ArrayValue 
    [DataContract("ArrayValue")]
    [KnownType(Proficy.Historian.ClientAccess.API.ElementValue)]
    [Serializable()]
    public ref class ArrayValue 
    Inheritance Hierarchy

    System.Object
       Proficy.Historian.ClientAccess.API.ArrayValue

    Requirements

    Target Platforms: Windows 7, Windows Vista SP1 or later, Windows XP SP3, Windows Server 2008 (Server Core not supported), Windows Server 2008 R2 (Server Core supported with SP1 or later), Windows Server 2003 SP2

    See Also