Represents details of individual archive files in a Historian server. Archives are multi-megabyte files
containing data between well defined start and end times. A constraint of the server does not allow two
or more archives to exist with overlapping start or end times.
System.Object
Proficy.Historian.ClientAccess.API.Archive
Target Platforms: Windows 7, Windows Vista SP1 or later, Windows XP SP3, Windows Server 2008 (Server Core not supported), Windows Server 2008 R2 (Server Core supported with SP1 or later), Windows Server 2003 SP2