Proficy Historian Client Access API
Proficy.Historian.ClientAccess.API Namespace / Collector Class / RedundancyFailoverOnBadQuality Property



In This Topic
    RedundancyFailoverOnBadQuality Property
    In This Topic
    Whether automatic failover occurs based on value quality of a watchdog tag in a collector redundancy configuration. When true, a Historian server will initiate failover to a backup collector if the latest received watchdog tag value has quality equal to DataQuality.StatusType.Bad.
    Syntax
    'Declaration
     
    Public Property RedundancyFailoverOnBadQuality As Boolean
    'Usage
     
    Dim instance As Collector
    Dim value As Boolean
     
    instance.RedundancyFailoverOnBadQuality = value
     
    value = instance.RedundancyFailoverOnBadQuality
    public bool RedundancyFailoverOnBadQuality {get; set;}
    public:
    property bool RedundancyFailoverOnBadQuality {
       bool get();
       void set (    bool value);
    }
    Requirements

    Target Platforms: Windows 7, Windows Vista SP1 or later, Windows XP SP3, Windows Server 2008 (Server Core not supported), Windows Server 2008 R2 (Server Core supported with SP1 or later), Windows Server 2003 SP2

    See Also