Proficy Historian Client Access API
Proficy.Historian.ClientAccess.API Namespace / Collector Class / Name Property



In This Topic
    Name Property (Collector)
    In This Topic
    A collector name. Collector names are unique within a single Historian server.
    Syntax
    'Declaration
     
    Public Property Name As String
    'Usage
     
    Dim instance As Collector
    Dim value As String
     
    instance.Name = value
     
    value = instance.Name
    public string Name {get; set;}
    public:
    property String^ Name {
       String^ get();
       void set (    String^ value);
    }
    Requirements

    Target Platforms: Windows 7, Windows Vista SP1 or later, Windows XP SP3, Windows Server 2008 (Server Core not supported), Windows Server 2008 R2 (Server Core supported with SP1 or later), Windows Server 2003 SP2

    See Also