Proficy Historian Client Access API
Proficy.Historian.ClientAccess.API Namespace / Collector Class / RedundancyPrincipalCollector Property



In This Topic
    RedundancyPrincipalCollector Property
    In This Topic
    A name of the collector backed up in a collector redundancy configuration. A collector will be next to become active for purposes of data collection should the system failover it's principal collector.
    Syntax
    'Declaration
     
    Public Property RedundancyPrincipalCollector As String
    'Usage
     
    Dim instance As Collector
    Dim value As String
     
    instance.RedundancyPrincipalCollector = value
     
    value = instance.RedundancyPrincipalCollector
    public string RedundancyPrincipalCollector {get; set;}
    public:
    property String^ RedundancyPrincipalCollector {
       String^ get();
       void set (    String^ value);
    }
    Requirements

    Target Platforms: Windows 7, Windows Vista SP1 or later, Windows XP SP3, Windows Server 2008 (Server Core not supported), Windows Server 2008 R2 (Server Core supported with SP1 or later), Windows Server 2003 SP2

    See Also