Proficy Historian Client Access API
Proficy.Historian.ClientAccess.API Namespace / Collector Class / DefaultSpikeInterval Property



In This Topic
    DefaultSpikeInterval Property
    In This Topic
    A spike interval value applied to newly added collector tags.
    Syntax
    'Declaration
     
    Public Property DefaultSpikeInterval As UInteger
    'Usage
     
    Dim instance As Collector
    Dim value As UInteger
     
    instance.DefaultSpikeInterval = value
     
    value = instance.DefaultSpikeInterval
    public uint DefaultSpikeInterval {get; set;}
    public:
    property uint DefaultSpikeInterval {
       uint get();
       void set (    uint value);
    }
    Requirements

    Target Platforms: Windows 7, Windows Vista SP1 or later, Windows XP SP3, Windows Server 2008 (Server Core not supported), Windows Server 2008 R2 (Server Core supported with SP1 or later), Windows Server 2003 SP2

    See Also