Proficy Historian Client Access API
Proficy.Historian.ClientAccess.API Namespace / Collector Class / DefaultCompressionTimeout Property



In This Topic
    DefaultCompressionTimeout Property
    In This Topic
    A collector compression timeout value applied to newly added collector tags.
    Syntax
    'Declaration
     
    Public Property DefaultCompressionTimeout As UInteger
    'Usage
     
    Dim instance As Collector
    Dim value As UInteger
     
    instance.DefaultCompressionTimeout = value
     
    value = instance.DefaultCompressionTimeout
    public uint DefaultCompressionTimeout {get; set;}
    public:
    property uint DefaultCompressionTimeout {
       uint get();
       void set (    uint value);
    }
    Requirements

    Target Platforms: Windows 7, Windows Vista SP1 or later, Windows XP SP3, Windows Server 2008 (Server Core not supported), Windows Server 2008 R2 (Server Core supported with SP1 or later), Windows Server 2003 SP2

    See Also