Proficy Historian Client Access API
Proficy.Historian.ClientAccess.API Namespace / Collector Class / LastModified Property



In This Topic
    LastModified Property (Collector)
    In This Topic
    The time when the collector's configuration was last modified.
    Syntax
    'Declaration
     
    Public Property LastModified As Date
    'Usage
     
    Dim instance As Collector
    Dim value As Date
     
    instance.LastModified = value
     
    value = instance.LastModified
    public DateTime LastModified {get; set;}
    public:
    property DateTime LastModified {
       DateTime get();
       void set (    DateTime value);
    }
    Requirements

    Target Platforms: Windows 7, Windows Vista SP1 or later, Windows XP SP3, Windows Server 2008 (Server Core not supported), Windows Server 2008 R2 (Server Core supported with SP1 or later), Windows Server 2003 SP2

    See Also