Proficy Historian Client Access API
Proficy.Historian.ClientAccess.API Namespace / Collector Class / Collector Constructor / Collector Constructor(Collector)
The source collector to copy.



In This Topic
    Collector Constructor(Collector)
    In This Topic
    Copy constructor.
    Syntax
    'Declaration
     
    Public Function New( _
       ByVal collector As Collector _
    )
    'Usage
     
    Dim collector As Collector
     
    Dim instance As New Collector(collector)
    public Collector( 
       Collector collector
    )
    public:
    Collector( 
       Collector^ collector
    )

    Parameters

    collector
    The source collector to copy.
    Requirements

    Target Platforms: Windows 7, Windows Vista SP1 or later, Windows XP SP3, Windows Server 2008 (Server Core not supported), Windows Server 2008 R2 (Server Core supported with SP1 or later), Windows Server 2003 SP2

    See Also