Proficy Historian Client Access API
Proficy.Historian.ClientAccess.API Namespace / Collector Class / RedundancyIsActiveCollector Property



In This Topic
    RedundancyIsActiveCollector Property
    In This Topic
    Whether this is the active collector for purposes of data collection in a collector redundancy configuration.
    Syntax
    'Declaration
     
    Public Property RedundancyIsActiveCollector As Boolean
    'Usage
     
    Dim instance As Collector
    Dim value As Boolean
     
    instance.RedundancyIsActiveCollector = value
     
    value = instance.RedundancyIsActiveCollector
    public bool RedundancyIsActiveCollector {get; set;}
    public:
    property bool RedundancyIsActiveCollector {
       bool get();
       void set (    bool value);
    }
    Requirements

    Target Platforms: Windows 7, Windows Vista SP1 or later, Windows XP SP3, Windows Server 2008 (Server Core not supported), Windows Server 2008 R2 (Server Core supported with SP1 or later), Windows Server 2003 SP2

    See Also