'Declaration Public Property DefaultLoadBalancing As Boolean
'Usage Dim instance As Collector Dim value As Boolean instance.DefaultLoadBalancing = value value = instance.DefaultLoadBalancing
public bool DefaultLoadBalancing {get; set;}
public: property bool DefaultLoadBalancing { bool get(); void set ( bool value); }
Target Platforms: Windows 7, Windows Vista SP1 or later, Windows XP SP3, Windows Server 2008 (Server Core not supported), Windows Server 2008 R2 (Server Core supported with SP1 or later), Windows Server 2003 SP2
Collector Class Collector Members