'Declaration Public Property DefaultCollectionInterval As UInteger
'Usage Dim instance As Collector Dim value As UInteger instance.DefaultCollectionInterval = value value = instance.DefaultCollectionInterval
public uint DefaultCollectionInterval {get; set;}
public: property uint DefaultCollectionInterval { uint get(); void set ( uint value); }
Target Platforms: Windows 7, Windows Vista SP1 or later, Windows XP SP3, Windows Server 2008 (Server Core not supported), Windows Server 2008 R2 (Server Core supported with SP1 or later), Windows Server 2003 SP2
Collector Class Collector Members