Proficy Historian Client Access API
Proficy.Historian.ClientAccess.API Namespace / Collector Class / RedundancyValueMaxUnchangedPeriod Property



In This Topic
    RedundancyValueMaxUnchangedPeriod Property
    In This Topic
    The maximum number of seconds a watchdog tag value can remain unchanged before failover is initiated.
    Syntax
    'Declaration
     
    Public Property RedundancyValueMaxUnchangedPeriod As UInteger
    'Usage
     
    Dim instance As Collector
    Dim value As UInteger
     
    instance.RedundancyValueMaxUnchangedPeriod = value
     
    value = instance.RedundancyValueMaxUnchangedPeriod
    public uint RedundancyValueMaxUnchangedPeriod {get; set;}
    public:
    property uint RedundancyValueMaxUnchangedPeriod {
       uint get();
       void set (    uint value);
    }
    Requirements

    Target Platforms: Windows 7, Windows Vista SP1 or later, Windows XP SP3, Windows Server 2008 (Server Core not supported), Windows Server 2008 R2 (Server Core supported with SP1 or later), Windows Server 2003 SP2

    See Also