Proficy Historian Client Access API
Proficy.Historian.ClientAccess.API Namespace / Collector Class / DefaultAbsoluteDeadbanding Property



In This Topic
    DefaultAbsoluteDeadbanding Property
    In This Topic
    Whether collector compression is expressed as an absolute value (true) or percent of engineering units for newly added collector tags.
    Syntax
    'Declaration
     
    Public Property DefaultAbsoluteDeadbanding As Boolean
    'Usage
     
    Dim instance As Collector
    Dim value As Boolean
     
    instance.DefaultAbsoluteDeadbanding = value
     
    value = instance.DefaultAbsoluteDeadbanding
    public bool DefaultAbsoluteDeadbanding {get; set;}
    public:
    property bool DefaultAbsoluteDeadbanding {
       bool get();
       void set (    bool value);
    }
    Requirements

    Target Platforms: Windows 7, Windows Vista SP1 or later, Windows XP SP3, Windows Server 2008 (Server Core not supported), Windows Server 2008 R2 (Server Core supported with SP1 or later), Windows Server 2003 SP2

    See Also