Proficy Historian Client Access API
Proficy.Historian.ClientAccess.API Namespace / Collector Class / Status Property



In This Topic
    Status Property (Collector)
    In This Topic
    An operational status of a collector.
    Syntax
    'Declaration
     
    Public Property Status As Collector.StatusType
    'Usage
     
    Dim instance As Collector
    Dim value As Collector.StatusType
     
    instance.Status = value
     
    value = instance.Status
    public Collector.StatusType Status {get; set;}
    public:
    property Collector.StatusType Status {
       Collector.StatusType get();
       void set (    Collector.StatusType value);
    }
    Requirements

    Target Platforms: Windows 7, Windows Vista SP1 or later, Windows XP SP3, Windows Server 2008 (Server Core not supported), Windows Server 2008 R2 (Server Core supported with SP1 or later), Windows Server 2003 SP2

    See Also