Proficy Historian Client Access API
Proficy.Historian.ClientAccess.API Namespace / IDataSamples Interface / HaveComments Method



In This Topic
    HaveComments Method (IDataSamples)
    In This Topic
    Whether data value comment records are provided.
    Syntax
    'Declaration
     
    Function HaveComments() As Boolean
    'Usage
     
    Dim instance As IDataSamples
    Dim value As Boolean
     
    value = instance.HaveComments()
    bool HaveComments()
    bool HaveComments(); 

    Return Value

    True if this instance includes data value comment records.
    Requirements

    Target Platforms: Windows 7, Windows Vista SP1 or later, Windows XP SP3, Windows Server 2008 (Server Core not supported), Windows Server 2008 R2 (Server Core supported with SP1 or later), Windows Server 2003 SP2

    See Also