Proficy Historian Client Access API
Proficy.Historian.ClientAccess.API Namespace / IDataSamples Interface / Count Method



In This Topic
    Count Method (IDataSamples)
    In This Topic
    Return a count of data values.
    Syntax
    'Declaration
     
    Function Count() As Integer
    'Usage
     
    Dim instance As IDataSamples
    Dim value As Integer
     
    value = instance.Count()
    int Count()
    int Count(); 

    Return Value

    Number of data values.
    Requirements

    Target Platforms: Windows 7, Windows Vista SP1 or later, Windows XP SP3, Windows Server 2008 (Server Core not supported), Windows Server 2008 R2 (Server Core supported with SP1 or later), Windows Server 2003 SP2

    See Also