Proficy Historian Client Access API
Proficy.Historian.ClientAccess.API Namespace / IDataSamples Interface / GetTime Method
An index value.



In This Topic
    GetTime Method (IDataSamples)
    In This Topic
    Return the data value time at a specific index.
    Syntax
    'Declaration
     
    Function GetTime( _
       ByVal index As Integer _
    ) As Date
    'Usage
     
    Dim instance As IDataSamples
    Dim index As Integer
    Dim value As Date
     
    value = instance.GetTime(index)
    DateTime GetTime( 
       int index
    )
    DateTime GetTime( 
       int index
    ) 

    Parameters

    index
    An index value.

    Return Value

    A data value time.
    Requirements

    Target Platforms: Windows 7, Windows Vista SP1 or later, Windows XP SP3, Windows Server 2008 (Server Core not supported), Windows Server 2008 R2 (Server Core supported with SP1 or later), Windows Server 2003 SP2

    See Also