Proficy Historian Client Access API
Proficy.Historian.ClientAccess.API Namespace / IDataSamples Interface / AddValue Method
A data value.



In This Topic
    AddValue Method (IDataSamples)
    In This Topic
    Append the given data value to this instance.
    Syntax
    'Declaration
     
    Sub AddValue( _
       ByVal value As Object _
    ) 
    'Usage
     
    Dim instance As IDataSamples
    Dim value As Object
     
    instance.AddValue(value)
    void AddValue( 
       object value
    )
    void AddValue( 
       Object^ value
    ) 

    Parameters

    value
    A data value.
    Requirements

    Target Platforms: Windows 7, Windows Vista SP1 or later, Windows XP SP3, Windows Server 2008 (Server Core not supported), Windows Server 2008 R2 (Server Core supported with SP1 or later), Windows Server 2003 SP2

    See Also