Proficy Historian Client Access API
Proficy.Historian.ClientAccess.API Namespace / IDataSamples Interface / GetQuality Method
An index value.



In This Topic
    GetQuality Method (IDataSamples)
    In This Topic
    Return the data value quality at a specific index.
    Syntax
    'Declaration
     
    Function GetQuality( _
       ByVal index As Integer _
    ) As IDataQuality
    'Usage
     
    Dim instance As IDataSamples
    Dim index As Integer
    Dim value As IDataQuality
     
    value = instance.GetQuality(index)
    IDataQuality GetQuality( 
       int index
    )
    IDataQuality^ GetQuality( 
       int index
    ) 

    Parameters

    index
    An index value.

    Return Value

    A data value quality.
    Requirements

    Target Platforms: Windows 7, Windows Vista SP1 or later, Windows XP SP3, Windows Server 2008 (Server Core not supported), Windows Server 2008 R2 (Server Core supported with SP1 or later), Windows Server 2003 SP2

    See Also