Proficy Historian Client Access API
Proficy.Historian.ClientAccess.API Namespace / IDataSamples Interface / Values Method



In This Topic
    Values Method
    In This Topic
    Return an array of data values.
    Syntax
    'Declaration
     
    Function Values() As Array
    'Usage
     
    Dim instance As IDataSamples
    Dim value As Array
     
    value = instance.Values()
    Array Values()
    Array^ Values(); 

    Return Value

    An array of data values.
    Requirements

    Target Platforms: Windows 7, Windows Vista SP1 or later, Windows XP SP3, Windows Server 2008 (Server Core not supported), Windows Server 2008 R2 (Server Core supported with SP1 or later), Windows Server 2003 SP2

    See Also