Proficy Historian Client Access API
Proficy.Historian.ClientAccess.API Namespace / ICollectors Interface / GetStatistics Method
A collector name.



In This Topic
    GetStatistics Method (ICollectors)
    In This Topic
    Retrieve statistics for a collector from a Historian server.
    Syntax
    'Declaration
     
    Function GetStatistics( _
       ByVal collectorname As String _
    ) As CollectorStatistics
    'Usage
     
    Dim instance As ICollectors
    Dim collectorname As String
    Dim value As CollectorStatistics
     
    value = instance.GetStatistics(collectorname)
    CollectorStatistics GetStatistics( 
       string collectorname
    )
    CollectorStatistics^ GetStatistics( 
       String^ collectorname
    ) 

    Parameters

    collectorname
    A collector name.

    Return Value

    Set of collector statistics.
    Requirements

    Target Platforms: Windows 7, Windows Vista SP1 or later, Windows XP SP3, Windows Server 2008 (Server Core not supported), Windows Server 2008 R2 (Server Core supported with SP1 or later), Windows Server 2003 SP2

    See Also