Proficy Historian Client Access API
Proficy.Historian.ClientAccess.API Namespace / ICollectors Interface / Unsubscribe Method
A collector name.



In This Topic
    Unsubscribe Method (ICollectors)
    In This Topic
    Unsubscribe to collector changes for a specific collector.
    Syntax
    'Declaration
     
    Sub Unsubscribe( _
       ByVal collectorname As String _
    ) 
    'Usage
     
    Dim instance As ICollectors
    Dim collectorname As String
     
    instance.Unsubscribe(collectorname)
    void Unsubscribe( 
       string collectorname
    )
    void Unsubscribe( 
       String^ collectorname
    ) 

    Parameters

    collectorname
    A collector name.
    Requirements

    Target Platforms: Windows 7, Windows Vista SP1 or later, Windows XP SP3, Windows Server 2008 (Server Core not supported), Windows Server 2008 R2 (Server Core supported with SP1 or later), Windows Server 2003 SP2

    See Also