Proficy Historian Client Access API
Proficy.Historian.ClientAccess.API Namespace / ICollectors Interface / UnsubscribeAny Method



In This Topic
    UnsubscribeAny Method (ICollectors)
    In This Topic
    Unsubscribe to collector changes for any collector.
    Syntax
    'Declaration
     
    Sub UnsubscribeAny() 
    'Usage
     
    Dim instance As ICollectors
     
    instance.UnsubscribeAny()
    void UnsubscribeAny()
    void UnsubscribeAny(); 
    Requirements

    Target Platforms: Windows 7, Windows Vista SP1 or later, Windows XP SP3, Windows Server 2008 (Server Core not supported), Windows Server 2008 R2 (Server Core supported with SP1 or later), Windows Server 2003 SP2

    See Also