Proficy Historian Client Access API
Proficy.Historian.ClientAccess.API Namespace / ICollectors Interface / Browse Method
A collector name.
Browse position.
Wildcard expression matching tag descriptions.
Wildcard expression matching source addresses.
Whether to recurse.



In This Topic
    Browse Method
    In This Topic
    Initiate a tag browse in a collector via a Historian server.
    Syntax
    'Declaration
     
    Sub Browse( _
       ByVal collectorname As String, _
       ByVal position As String, _
       ByVal descriptionmask As String, _
       ByVal addressmask As String, _
       ByVal recursive As Boolean _
    ) 
    'Usage
     
    Dim instance As ICollectors
    Dim collectorname As String
    Dim position As String
    Dim descriptionmask As String
    Dim addressmask As String
    Dim recursive As Boolean
     
    instance.Browse(collectorname, position, descriptionmask, addressmask, recursive)
    void Browse( 
       string collectorname,
       string position,
       string descriptionmask,
       string addressmask,
       bool recursive
    )
    void Browse( 
       String^ collectorname,
       String^ position,
       String^ descriptionmask,
       String^ addressmask,
       bool recursive
    ) 

    Parameters

    collectorname
    A collector name.
    position
    Browse position.
    descriptionmask
    Wildcard expression matching tag descriptions.
    addressmask
    Wildcard expression matching source addresses.
    recursive
    Whether to recurse.
    Requirements

    Target Platforms: Windows 7, Windows Vista SP1 or later, Windows XP SP3, Windows Server 2008 (Server Core not supported), Windows Server 2008 R2 (Server Core supported with SP1 or later), Windows Server 2003 SP2

    See Also