Proficy Historian Client Access API
Proficy.Historian.ClientAccess.API Namespace / ICollectors Interface / CollectorBrowseResponseEvent Event



In This Topic
    CollectorBrowseResponseEvent Event (ICollectors)
    In This Topic
    Occurs when a collector responds with tag browse information.
    Syntax
    'Declaration
     
    Event CollectorBrowseResponseEvent As CollectorBrowseResponseHandler
    'Usage
     
    Dim instance As ICollectors
    Dim handler As CollectorBrowseResponseHandler
     
    AddHandler instance.CollectorBrowseResponseEvent, handler
    event CollectorBrowseResponseHandler CollectorBrowseResponseEvent
    event CollectorBrowseResponseHandler^ CollectorBrowseResponseEvent
    Requirements

    Target Platforms: Windows 7, Windows Vista SP1 or later, Windows XP SP3, Windows Server 2008 (Server Core not supported), Windows Server 2008 R2 (Server Core supported with SP1 or later), Windows Server 2003 SP2

    See Also