Proficy Historian Client Access API
Proficy.Historian.ClientAccess.API Namespace / ICollectors Interface / InitiateFailover Method
A collector name



In This Topic
    InitiateFailover Method
    In This Topic
    Trigger a manual collector failover in a collector redundancy configuration via a Historian server. After failover a backup collector will take-over data collection for the currently active collector.
    Syntax
    'Declaration
     
    Sub InitiateFailover( _
       ByVal collectorname As String _
    ) 
    'Usage
     
    Dim instance As ICollectors
    Dim collectorname As String
     
    instance.InitiateFailover(collectorname)
    void InitiateFailover( 
       string collectorname
    )
    void InitiateFailover( 
       String^ collectorname
    ) 

    Parameters

    collectorname
    A collector name
    Requirements

    Target Platforms: Windows 7, Windows Vista SP1 or later, Windows XP SP3, Windows Server 2008 (Server Core not supported), Windows Server 2008 R2 (Server Core supported with SP1 or later), Windows Server 2003 SP2

    See Also