Proficy Historian Client Access API
Proficy.Historian.ClientAccess.API Namespace / DataQuality Class / IsReplaced Property



In This Topic
    IsReplaced Property
    In This Topic
    Whether the associated data value has been flagged as replaced.
    Syntax
    'Declaration
     
    Public ReadOnly Property IsReplaced As Boolean
    'Usage
     
    Dim instance As DataQuality
    Dim value As Boolean
     
    value = instance.IsReplaced
    public bool IsReplaced {get;}
    public:
    property bool IsReplaced {
       bool get();
    }
    Requirements

    Target Platforms: Windows 7, Windows Vista SP1 or later, Windows XP SP3, Windows Server 2008 (Server Core not supported), Windows Server 2008 R2 (Server Core supported with SP1 or later), Windows Server 2003 SP2

    See Also