Proficy Historian Client Access API
Proficy.Historian.ClientAccess.API Namespace / DataQuality Class / GetHashCode Method



In This Topic
    GetHashCode Method (DataQuality)
    In This Topic
    Returns the hash code for this instance.
    Syntax
    'Declaration
     
    Public Overrides Function GetHashCode() As Integer
    'Usage
     
    Dim instance As DataQuality
    Dim value As Integer
     
    value = instance.GetHashCode()
    public override int GetHashCode()
    public:
    int GetHashCode(); override 

    Return Value

    Hash code value of this instance.
    Requirements

    Target Platforms: Windows 7, Windows Vista SP1 or later, Windows XP SP3, Windows Server 2008 (Server Core not supported), Windows Server 2008 R2 (Server Core supported with SP1 or later), Windows Server 2003 SP2

    See Also