Proficy Historian Client Access API
Proficy.Historian.ClientAccess.API Namespace / DataQuality Class / UserStatus Property



In This Topic
    UserStatus Property
    In This Topic
    Optional, user-defined status bits.
    Syntax
    'Declaration
     
    Public Property UserStatus As UShort
    'Usage
     
    Dim instance As DataQuality
    Dim value As UShort
     
    instance.UserStatus = value
     
    value = instance.UserStatus
    public ushort UserStatus {get; set;}
    public:
    property ushort UserStatus {
       ushort get();
       void set (    ushort value);
    }
    Requirements

    Target Platforms: Windows 7, Windows Vista SP1 or later, Windows XP SP3, Windows Server 2008 (Server Core not supported), Windows Server 2008 R2 (Server Core supported with SP1 or later), Windows Server 2003 SP2

    See Also