Proficy Historian Client Access API
Proficy.Historian.ClientAccess.API Namespace / DataQuality Class / IsBad Property



In This Topic
    IsBad Property
    In This Topic
    Whether this instance is of DataQuality.StatusType.Bad quality.
    Syntax
    'Declaration
     
    Public Property IsBad As Boolean
    'Usage
     
    Dim instance As DataQuality
    Dim value As Boolean
     
    instance.IsBad = value
     
    value = instance.IsBad
    public bool IsBad {get; set;}
    public:
    property bool IsBad {
       bool get();
       void set (    bool value);
    }
    Requirements

    Target Platforms: Windows 7, Windows Vista SP1 or later, Windows XP SP3, Windows Server 2008 (Server Core not supported), Windows Server 2008 R2 (Server Core supported with SP1 or later), Windows Server 2003 SP2

    See Also