'Usage Dim instance As DataQuality Dim obj As Object Dim value As Boolean value = instance.Equals(obj)
Parameters
- obj
- An object to test.
Return Value
True if the specified object equals this instance.
'Usage Dim instance As DataQuality Dim obj As Object Dim value As Boolean value = instance.Equals(obj)
Target Platforms: Windows 7, Windows Vista SP1 or later, Windows XP SP3, Windows Server 2008 (Server Core not supported), Windows Server 2008 R2 (Server Core supported with SP1 or later), Windows Server 2003 SP2