Proficy Historian Client Access API
Proficy.Historian.ClientAccess.API Namespace / DataQuality Class / Substatus Property



In This Topic
    Substatus Property
    In This Topic
    Overall quality sub-status.
    Syntax
    'Declaration
     
    Public Property Substatus As DataQuality.SubstatusType
    'Usage
     
    Dim instance As DataQuality
    Dim value As DataQuality.SubstatusType
     
    instance.Substatus = value
     
    value = instance.Substatus
    public DataQuality.SubstatusType Substatus {get; set;}
    public:
    property DataQuality.SubstatusType Substatus {
       DataQuality.SubstatusType get();
       void set (    DataQuality.SubstatusType value);
    }
    Requirements

    Target Platforms: Windows 7, Windows Vista SP1 or later, Windows XP SP3, Windows Server 2008 (Server Core not supported), Windows Server 2008 R2 (Server Core supported with SP1 or later), Windows Server 2003 SP2

    See Also