Proficy Historian Client Access API
Proficy.Historian.ClientAccess.API Namespace / Archive Class / Filename Property



In This Topic
    Filename Property
    In This Topic
    An archive file name.
    Syntax
    'Declaration
     
    <DataMemberAttribute("File")>
    Public Property Filename As String
    'Usage
     
    Dim instance As Archive
    Dim value As String
     
    instance.Filename = value
     
    value = instance.Filename
    [DataMember("File")]
    public string Filename {get; set;}
    [DataMember("File")]
    public:
    property String^ Filename {
       String^ get();
       void set (    String^ value);
    }
    Requirements

    Target Platforms: Windows 7, Windows Vista SP1 or later, Windows XP SP3, Windows Server 2008 (Server Core not supported), Windows Server 2008 R2 (Server Core supported with SP1 or later), Windows Server 2003 SP2

    See Also