Proficy Historian Client Access API
Proficy.Historian.ClientAccess.API Namespace / Archive Class / DataStoreName Property



In This Topic
    DataStoreName Property (Archive)
    In This Topic
    Name of the Data Store Name where this archive belong to
    Syntax
    'Declaration
     
    <DataMemberAttribute("DataStoreName")>
    Public Property DataStoreName As String
    'Usage
     
    Dim instance As Archive
    Dim value As String
     
    instance.DataStoreName = value
     
    value = instance.DataStoreName
    [DataMember("DataStoreName")]
    public string DataStoreName {get; set;}
    [DataMember("DataStoreName")]
    public:
    property String^ DataStoreName {
       String^ get();
       void set (    String^ value);
    }
    Requirements

    Target Platforms: Windows 7, Windows Vista SP1 or later, Windows XP SP3, Windows Server 2008 (Server Core not supported), Windows Server 2008 R2 (Server Core supported with SP1 or later), Windows Server 2003 SP2

    See Also