Proficy Historian Client Access API
Proficy.Historian.ClientAccess.API Namespace / Archive Class / LastModifiedUser Property



In This Topic
    LastModifiedUser Property (Archive)
    In This Topic
    A user name of the last user to update archive configuration.
    Syntax
    'Declaration
     
    <DataMemberAttribute("LastModifiedUser")>
    Public Property LastModifiedUser As String
    'Usage
     
    Dim instance As Archive
    Dim value As String
     
    instance.LastModifiedUser = value
     
    value = instance.LastModifiedUser
    [DataMember("LastModifiedUser")]
    public string LastModifiedUser {get; set;}
    [DataMember("LastModifiedUser")]
    public:
    property String^ LastModifiedUser {
       String^ get();
       void set (    String^ value);
    }
    Requirements

    Target Platforms: Windows 7, Windows Vista SP1 or later, Windows XP SP3, Windows Server 2008 (Server Core not supported), Windows Server 2008 R2 (Server Core supported with SP1 or later), Windows Server 2003 SP2

    See Also