Proficy Historian Client Access API
Proficy.Historian.ClientAccess.API Namespace / Archive Class / IsEndTimeFixed Property



In This Topic
    IsEndTimeFixed Property
    In This Topic
    Whether the archive has end time fixed.
    Syntax
    'Declaration
     
    <DataMemberAttribute("IsEndTimeFixed")>
    Public Property IsEndTimeFixed As Boolean
    'Usage
     
    Dim instance As Archive
    Dim value As Boolean
     
    instance.IsEndTimeFixed = value
     
    value = instance.IsEndTimeFixed
    [DataMember("IsEndTimeFixed")]
    public bool IsEndTimeFixed {get; set;}
    [DataMember("IsEndTimeFixed")]
    public:
    property bool IsEndTimeFixed {
       bool get();
       void set (    bool value);
    }
    Requirements

    Target Platforms: Windows 7, Windows Vista SP1 or later, Windows XP SP3, Windows Server 2008 (Server Core not supported), Windows Server 2008 R2 (Server Core supported with SP1 or later), Windows Server 2003 SP2

    See Also