Proficy Historian Client Access API
Proficy.Historian.ClientAccess.API Namespace / IServer Interface / GetTimeZoneStandardName Method


GetTimeZoneStandardName Method
Retrieve the standard name of the time zone local to a Historian server.
Syntax
Function GetTimeZoneStandardName() As System.String

Return Value

A time zone standard name.
Requirements

Target Platforms: Windows 7, Windows Vista SP1 or later, Windows XP SP3, Windows Server 2008 (Server Core not supported), Windows Server 2008 R2 (Server Core supported with SP1 or later), Windows Server 2003 SP2

See Also